FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Auto tuning
FAQ
Auto tuning
I started auto tuning in the PU operation mode.
However, the RUN LED blinks and monitor indicator remains as "1".
The auto tuning parameters have already been set and the monitor shows "1".
However, the RUN LED blinks and monitor indicator remains as "1".
The auto tuning parameters have already been set and the monitor shows "1".
- Category :
Answer
Check if any device is connected to the inverter's external terminal.
In particular, check if MRS and SD are short-circuited.
If they are short-circuited, open them.
In particular, check if MRS and SD are short-circuited.
If they are short-circuited, open them.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700