FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Frequency setting
FAQ
Frequency setting
I use the CC-Link option FR-A7NC to set the frequency to 60 Hz, but the monitor value is shown as "60.09 Hz" when the inverter operates.
Can I adjust it to 60 Hz?
Can I adjust it to 60 Hz?
- Category :
Answer
Since the Advanced magnetic flux vector control method uses slip compensation to compensate the frequency, the value is not shown as exactly 60 Hz.
For V/F control, check if slip compensation is enabled.
For V/F control, check if slip compensation is enabled.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700