FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Encoder cable length restriction
FAQ
Encoder cable length restriction
Can I use the encoder cable FR-VCBL150M for a combination of the FR-V200E (amplifier) and SF-VR (motor)?
- Category :
Answer
If the cable length is longer than 100 m, speed may not be read correctly due to voltage drop and waveform deformation of the encoder signal. Therefore, use the wiring length of up to 100 m.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200