FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Coasting to stop method
FAQ
Coasting to stop method
How can I perform coasting to stop with the combination of the FR-V200 and dedicated motor?
According to description in the manual, the FR-V200 does not have the terminal MRS.
According to description in the manual, the FR-V200 does not have the terminal MRS.
- Category :
Answer
Use Pr.17 (Input terminal assignment) to assign MRS to the terminals DI1, DI2, and DI3.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200