FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Terminal FM
FAQ
Terminal FM
The terminal FM is usually used to connect a 1 mA full-scale ammeter. Can I connect a 0 to 10 V speedometer to this terminal? (To display the maximum frequency of 60 Hz when 10 V is applied)
- Category :
Answer
Since the terminal FM is designed with 8 V peak pulse voltage output, it cannot output 10 V.
Since the terminal AM is an analog output of 0 V to 10 V, use this instead.
Since the terminal AM is an analog output of 0 V to 10 V, use this instead.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500