FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Reset selection
FAQ
Reset selection
Why does not the FR-V200E series allow for choosing from "Reset input always enabled" and "Reset input enabled only when the protective function is activated" (Pr.75) as the FR-A500 does?
How can I use "Reset input always enabled"?
How can I use "Reset input always enabled"?
- Category :
Answer
The specifications of the FR-V200E series do not allow for choosing from "Reset input always enabled" and "Reset input enabled only when the protective function is activated" as you mention.
By connecting the wires for the inverter's fault output NO, NC, and transfer contacts to the reset signal wire in series, you can achieve "Reset input enabled only when the protective function is activated".
Design the circuit in this way.
By connecting the wires for the inverter's fault output NO, NC, and transfer contacts to the reset signal wire in series, you can achieve "Reset input enabled only when the protective function is activated".
Design the circuit in this way.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200