FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Vector inverter option
FAQ
Vector inverter option
I want to use only the encoder output of the additional I/O function FR-VPA. Are pulses output when the motor rotates after just adding the option?
- Category :
Answer
Just by adding this option, encoder pulses connected to the inverter or option are output.
You can also divide the pulse train output.
You can also divide the pulse train output.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- FR-V200