FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Can I drive multiple motors with a single inverter?
FAQ
Can I drive multiple motors with a single inverter?
Can I drive two 0.4 kW motors and one 0.1 kW motor with a single inverter?
- Category :
Answer
You can drive multiple motors with a single inverter.
However, since the inverter cannot determine the current of each motor, the electronic thermal O/L relay cannot be used.
Therefore, you need to attach an external thermal for each motor for protection.
However, since the inverter cannot determine the current of each motor, the electronic thermal O/L relay cannot be used.
Therefore, you need to attach an external thermal for each motor for protection.
- Product Name
- Inverter, magnet motor drive
- Series
- Others