FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Inverter communication
FAQ
Inverter communication
I want to use the inverter setup software to save parameters, but cannot establish communication.
Let me know details of the system configuration, communication setting, and environmental setting.
The inverter has no option installed.
Let me know details of the system configuration, communication setting, and environmental setting.
The inverter has no option installed.
- Category :
Answer
Check if the communication setting parameters (Pr.117 to Pr.124) are set to the same values between the inverter and personal computer.
Note that communication is not established if Pr.122 (Communication check time interval) is set to "0" (initial setting). Be sure to change this parameter setting.
Note that communication is not established if Pr.122 (Communication check time interval) is set to "0" (initial setting). Be sure to change this parameter setting.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500