FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regardng compatability with other product series
FAQ
Regardng compatability with other product series
FX5 CPU modules
can FX2N series I/O modules (or extension modules) be connected?
Can FX2 intelligent function modules be connected?
Can FX3 special adapters be connected?
Can FX3 intelligent function modules be connected?
can FX2N series I/O modules (or extension modules) be connected?
Can FX2 intelligent function modules be connected?
Can FX3 special adapters be connected?
Can FX3 intelligent function modules be connected?
Answer
Although the connection with FX2N series I/O modules, FX2 series intelligent function modules, and FX3 series special adater is not possible, FX3 series intelligent function modules can be connected with FX5 CPU modules.
However, bus conversion module is required. (FX5-CNV-BUS/FX5-CNV-BUSC).
You can check the device configuration of the FX5 CPU module with the model selection tool.
However, bus conversion module is required. (FX5-CNV-BUS/FX5-CNV-BUSC).
You can check the device configuration of the FX5 CPU module with the model selection tool.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, I/O Module
- Series
- MELSEC iQ-F Series