FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > Accessories of the MELSEC iQ-R series 40-pin connector type module
FAQ
Accessories of the MELSEC iQ-R series 40-pin connector type module
Is a connector provided with a MELSEC iQ-R series 40-pin connector type module?
- Category :
Answer
No connector is provided with the module. Separately prepare any of the following connectors.
A6CON1: Soldering type 32-point connector (40-pin connector)
A6CON2: Crimp contact type 32-point connector (40-pin connector)
A6CON3: Flat cable pressure welding type 32-point connector (40-pin connector)
A6CON4: Soldering type 32-point connector (40-pin connector, cable connectable in bidirection)
A6CON1: Soldering type 32-point connector (40-pin connector)
A6CON2: Crimp contact type 32-point connector (40-pin connector)
A6CON3: Flat cable pressure welding type 32-point connector (40-pin connector)
A6CON4: Soldering type 32-point connector (40-pin connector, cable connectable in bidirection)
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series