FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > I cannot place a main base unit in a module configuration diagram with GX Works3.
FAQ
I cannot place a main base unit in a module configuration diagram with GX Works3.
I cannot place a main base unit in a module configuration diagram with GX Works3.
- Category :
Answer
You may have already placed a main base unit in the module configuration diagram.
Scroll up or down in the module configuration diagram and check if a main base unit has been placed in it.
When it has already been placed, you can place a new main base unit after deleting the existing main base unit.
Scroll up or down in the module configuration diagram and check if a main base unit has been placed in it.
When it has already been placed, you can place a new main base unit after deleting the existing main base unit.
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series
May I have your opinion?
Related FAQ
- Combination of the MELSEC iQ-R series inter-module synchronization function and the CC-Link IE Field Network synchronous communication function
- Built-in Ethernet function setting window of MELSEC iQ-R series CPU modules
- Number of modules that can be synchronized using the MELSEC iQ-R series inter-module synchronization function
- Security functions of MELSEC iQ-R series
- OS compatible with GX Works3