FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > Combination of the MELSEC iQ-R series inter-module synchronization function and the CC-Link IE Field Network synchronous communication function
FAQ
Combination of the MELSEC iQ-R series inter-module synchronization function and the CC-Link IE Field Network synchronous communication function
How can I use the MELSEC iQ-R series inter-module synchronization function together with the CC-Link IE Field Network synchronous communication function?
- Category :
Answer
In the communication of the CC-Link IE Field Network synchronous communication function, you can synchronize the timing
to send/receive data with the inter-module synchronization cycle of the inter-module synchronization function.
With this synchronization, the inter-module synchronization timing of the master station's system is sent to local stations via
the network, and local station send the inter-module synchronization cycle timing to each module in its own system.
to send/receive data with the inter-module synchronization cycle of the inter-module synchronization function.
With this synchronization, the inter-module synchronization timing of the master station's system is sent to local stations via
the network, and local station send the inter-module synchronization cycle timing to each module in its own system.
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series