FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > Combination of the MELSEC iQ-R series inter-module synchronization function and the fixed scan communication of the multiple CPU system function
FAQ
Combination of the MELSEC iQ-R series inter-module synchronization function and the fixed scan communication of the multiple CPU system function
How can I use the MELSEC iQ-R series inter-module synchronization function together with the fixed scan communication cycle of the multiple CPU system function?
- Category :
Answer
You can synchronize the fixed scan communication cycle of the multiple CPU system function with the inter-module synchronization
cycle of the inter-module synchronization function.
With this synchronization, modules with different control CPUs can be synchronously operated.
cycle of the inter-module synchronization function.
With this synchronization, modules with different control CPUs can be synchronously operated.
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series