FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Reading project data from a CD-R
FAQ
Reading project data from a CD-R
Project data of GX Developer on a CD-R cannot be reopened after the data is written to the CD-R. How can I read it?
- Category :
Answer
To reopen project data written to a CD-R, copy the project data into a space such as a hard disk on the personal computer where the project data is used.
This operation is required because GX Developer executes data writing when a project is opened.
A project folder copied into a HD is set to "read only". Uncheck the "read only" box.
This operation is required because GX Developer executes data writing when a project is opened.
A project folder copied into a HD is set to "read only". Uncheck the "read only" box.
- Product Name
- Engineering Software
- Series
- Software Package (GPP function)