FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Writing QJ71C24N's parameters in GX Works2
FAQ
Writing QJ71C24N's parameters in GX Works2
When are the switch setting and the settings of "Various Control Specifications" for the QJ71C4N series intelligent function modules written by GX Works2?
- Category :
Answer
The switch setting is written when CPU module's parameters are written. The settings of "Various Control Specifications" are written when intelligent function module settings are written.
- Product Name
- Engineering Software
- Series
- Software Package (GPP function)