FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > GX Works2's compatibility with the ACPU modules
FAQ
GX Works2's compatibility with the ACPU modules
Does GX Works2 support the ACPU modules?
- Category :
Answer
GX Works2 does not support the ACPU modules.
Use GX Developer for the ACPU modules.
GX Developer is included on the CD-ROM of GX Works2.
For the installation procedure, refer to the following manuals.
GX Works2 Version 1 Operating Manual (Common)
Model code: 13JU64
Appendix 14 Procedure to Use GX Works2 Unsupported Programmable Controller Type
Use GX Developer for the ACPU modules.
GX Developer is included on the CD-ROM of GX Works2.
For the installation procedure, refer to the following manuals.
GX Works2 Version 1 Operating Manual (Common)
Model code: 13JU64
Appendix 14 Procedure to Use GX Works2 Unsupported Programmable Controller Type
- Product Name
- Engineering Software
- Series
- Software Package (GPP function)