FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Using GX Logviewer's realtime monitor function on multiple personal computers
FAQ
Using GX Logviewer's realtime monitor function on multiple personal computers
Is it possible to use the realtime monitor function of GX Logviewer on multiple personal computers?
- Category :
Answer
Up to two realtime monitor windows can be used for monitoring.
If each of two personal computers monitors one monitor window, two personal computers can be connected.
If a single personal computer monitors two windows, one personal computer can be connected.
If each of two personal computers monitors one monitor window, two personal computers can be connected.
If a single personal computer monitors two windows, one personal computer can be connected.
- Product Name
- Engineering Software
- Series
- Software Package (other functions)