FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Adding statements to SFC programs
FAQ
Adding statements to SFC programs
Is it possible to add statements to an SFC ladder program created in a simple project?
- Category :
Answer
No statements can be added. Please add notes or comments instead.
- Product Name
- Engineering Software
- Series
- Software Package (GPP function)
May I have your opinion?
Related FAQ
- Compatibility of the high speed data logger module's report function with 64-bit Excel2010
- MX Component Version 4's compatibility with Visual Basic .NET 2003
- MX Sheet Version 2's compatibility with 32-bit Excel2010
- Using send FBs/receive FBs simultaneously
- Required setting for the display of hidden comments