FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Time out error in the communication test of MX Component
FAQ
Time out error in the communication test of MX Component
When I use MX Component, a time out error occurs in the communication test with an Ethernet interface module. What is the cause of this error?
- Category :
Answer
The possible causes are as follows.
- Incorrect setting with a personal computer or an Ethernet interface module
Check the IP address, network number, station number, and other settings.
- Improper condition of the HUB or LAN cable
Check the connection of the LAN cable or the HUB for the power discontinuity.
- Incorrect setting of the communication setting utility
Check if the settings of the Ethernet interface module and the settings of the communication setting utility match.
- Incorrect setting with a personal computer or an Ethernet interface module
Check the IP address, network number, station number, and other settings.
- Improper condition of the HUB or LAN cable
Check the connection of the LAN cable or the HUB for the power discontinuity.
- Incorrect setting of the communication setting utility
Check if the settings of the Ethernet interface module and the settings of the communication setting utility match.
- Product Name
- Engineering Software
- Series
- Middleware