Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 38043
  • Release Date : 2021/02/25 17:54
  • Print

Checking the disconnection or communications error status of the Energy measuring Unit

Disconnection or communications error of the Energy Measuring Units connected to EcoWebServerIII can be detected?
Category : 

Answer

There is no way to detect a disconnection or communications error in the Energy measuring Unit.
As an alternative idea, we have two solutions to monitor the measuring points.
 
Solution 1: Having the measuring error information by contact outputs
By setting "Measuring Error" for the contact output conditions, you can find out that the measuring error occurred by contact outputs when you cannot collect measuring point data.
For the procedures, please refer to the User's manual 4.9.3. contact output settings.
 
Solution 2: Having the measuring error information by email notifications
By setting "Measuring Error" for the email notifications conditions, you can find out that the measuring error occurred by email notifications.
For the procedures, please refer to the User's manual 4.9.6. EcoWebServerIII error notification settings.
Product Name
Energy Saving Data Collecting Servers
Series
EcoWebServerIII
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?