FAQ


FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Saving Data Collecting Servers > Checking the IP address of EcoWebServerIII
FAQ
Checking the IP address of EcoWebServerIII
How to check the IP address of EcoWebServerIII?
Answer
(1) Open the front cover on the server section, and set the MODE switch to the "STOP" position.
(2) Set the RESET switch to the "SEL." position.
(3) After the "CF CARD" LED turns off, turn the RESET switch to the "RES."
(4) After all the LEDs except the "POWER" LED on the power supply section turn off, return the RESET switch to the central position.
(5) Wait until the product starts up and the IP address is displayed on the 7-segment LED at the front.
(2) Set the RESET switch to the "SEL." position.
(3) After the "CF CARD" LED turns off, turn the RESET switch to the "RES."
(4) After all the LEDs except the "POWER" LED on the power supply section turn off, return the RESET switch to the central position.
(5) Wait until the product starts up and the IP address is displayed on the 7-segment LED at the front.

- Product Name
- Energy Saving Data Collecting Servers
- Series
- EcoWebServerIII