FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the FX5S CPU Module Line-up
FAQ
Regarding the FX5S CPU Module Line-up
How many input and output point types does the FX5S CPU module have?
Answer
The line-up of input and output points of the FX5S CPU module is as follows.
・30 points (Input: 16 points, Output: 14 points)
・40 points (Input: 24 points, Output: 16 points)
・60 points (Input: 36 points, Output: 24 points)
・30 points (Input: 16 points, Output: 14 points)
・40 points (Input: 24 points, Output: 16 points)
・60 points (Input: 36 points, Output: 24 points)
- Product Name
- FX5S
- Product Category
- CPU Module
- Series
- MELSEC iQ-F Series