FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding FX5U/FX5UC CPU Module Built-in functions
FAQ
Regarding FX5U/FX5UC CPU Module Built-in functions
When comparing the internal functions of the CPU Modules of the FX5S/FX5UJ and the FX5U/FX5UC, are there any functions supported only by the FX5U/FX5UC CPU Modules?
Answer
The functions supported only by the FX5U/FX5UC CPU Modules are listed below.
・Predefined Protocol Support Function For Positioning function
・Optional battery: FX3U-32BL connection (Battery adds latch area, retains clock data)
・Predefined Protocol Support Function For Positioning function
・Optional battery: FX3U-32BL connection (Battery adds latch area, retains clock data)
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module
- Series
- MELSEC iQ-F Series