Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 44331
  • Release Date : 2024/03/20 12:54
  • Print

Regarding specifications of the forced ON/OFF function for external input/output

Is there any difference in the forced ON/OFF function of external input/output between iQ-F series and iQ-R series?
Category : 

Answer

The following points are different for the iQ-F series.
・All output disabled flag (SM8034)
When SM8034 is ON, the all output disabled flag is given priority, so all output terminals are turned OFF regardless of forced ON/OFF registration, and only the forced ON/OFF is reflected on the output device.
・Non-latch memory all clear (SM8031)
If SM8031 is ON, forced ON/OFF will not be reflected.
・Memory hold stop (SM8033)
If SM8033 is ON, forced ON/OFF will not be reflected.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries