Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 44335
  • Release Date : 2024/03/20 13:21
  • Print

Regarding differences in specifications of the FTP server auto transfer function for data logging files

Is there any difference in the FTP server auto transfer function between the iQ-F series and the iQ-R series?
Category : 

Answer

The following points are different for the iQ-F series.
・Error History
 If the FX5 CPU Module is turned off, the error history is cleared.
・Setting details of the CPU Module Logging Configuration Tool
 DNS server settings are not supported.
・Directory
 If the specified directory does not exist on the FTP server, no error occurs and the directory is created and the file is transferred.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries