FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding reuse of GOT connector cable when replacing with FX5 CPU module
FAQ
Regarding reuse of GOT connector cable when replacing with FX5 CPU module
I use the RS422 port of the FX3U basic unit to connect the GOT serially. Can I use the same cable with the FX5U CPU module?
Answer
The connection cable is GT01-C30R4-8P. The FX5U CPU module does not have an RS422 port, so you will need to add an FX5-422-BD-GOT.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module
- Series
- MELSEC iQ-F Series
May I have your opinion?
Related FAQ
- Regarding number of servo amplifiers that can be connected via PDO communication
- Regarding How to release Online Program Change
- Regarding COM terminals of FX5-2HC/ES
- Regarding issuing Client Certificates to Connect with AWS IoT Core
- Regarding compatible version of CANopen communication function for PDO communication