FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Automation Controllers MELSEC > MELSEC MX Controller MX-F Model > Regarding maximum number of input/output points
FAQ
Regarding maximum number of input/output points
What is the maximum number of input/output points for the MX-F Model?
Answer
The maximum number of input/output points is 512.
The number of remote I/O points is not limited, but can be used within the specification range of each intelligent function module.
In addition, the MX-F Model does not have the number of I/O occupied points when the intelligent function module is connected, which was the case with the iQ-F series and the F series, so there is no need to consider it.
- Product Name
- MX-F Model
- Series
- MELSEC MX Controller