FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Automation Controllers MELSEC > MELSEC MX Controller MX-F Model > Regarding built-in high-speed counter function
FAQ
Regarding built-in high-speed counter function
The CPU Module of the iQ-F series supports the built-in high-speed counter function, but does the MX-F Model also support it?
Answer
The MX-F Model also supports the built-in high-speed counter function.
The number of channels is up to 8, and the counter types supported are 1-phase 1-input/1-phase 2-input/2-phase 2-input (1x/2x/4x)/internal clock (1MHz (fixed)).
The maximum frequency varies depending on the counter type, but up to 200kHz is supported.
- Product Name
- MX-F Model
- Series
- MELSEC MX Controller