FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A5AY
FAQ
FR-A5AY
When replacing the FR-A500 with FR-A700 (F700(P)), is the FR-A5AY that have been used in the FR-A500 available for the FR-A700 (F700(P)) ? Can it be mounted by mistake?
- Category :
Answer
The FR-A5AY cannot be used in the FR-A700 (F700(P)). It cannot be installed due to the difference of the connector shape.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-F700P, FR-F700