FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Magnetic flux vector control
FAQ
Magnetic flux vector control
The motor is SF-HRFCA.
I want to perform low-speed operation that requires short-time torque. Do I have to use (Advanced) magnetic flux vector control?
I want to perform low-speed operation that requires short-time torque. Do I have to use (Advanced) magnetic flux vector control?
- Category :
Answer
For low-speed operation, perform auto tuning and use (Advanced) magnetic flux vector control.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700