FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > CC-Link
FAQ
CC-Link
The RUN LED of the inverter blinks during CC-Link operation. What does this mean?
Pr.17 (MRS input selection) is set to "2", NC contact input specifications, for the terminal MRS.
Pr.17 (MRS input selection) is set to "2", NC contact input specifications, for the terminal MRS.
- Category :
Answer
Slow blinking of the RUN LED indicates reverse operation.
Fast blinking indicates that while the start command is input, the running frequency command is not set (for example, the setting value is lower than the starting frequency).
This state also occurs while the MRS signal is input.
Signal presence at the terminal MRS can be checked by setting Pr.52 (DU/PU main display data selection) to "55" (I/O terminal monitor).
Fast blinking indicates that while the start command is input, the running frequency command is not set (for example, the setting value is lower than the starting frequency).
This state also occurs while the MRS signal is input.
Signal presence at the terminal MRS can be checked by setting Pr.52 (DU/PU main display data selection) to "55" (I/O terminal monitor).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700