FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > CC-Link
FAQ
CC-Link
I am considering to use the CC-Link option FR-A7NC to operate the FR-E700. Can I use the CC-Link type programming example for the FR-E500 as a reference?
Are there any other good example programs on the Mitsubishi Electric FA Global Website?
Are there any other good example programs on the Mitsubishi Electric FA Global Website?
- Category :
Answer
You can use the CC-Link type programming example for the FR-E500 as a reference.
In the programming example for the FR-E500, the A series programmable controller is used.
The Instruction Manual of the FR-A7NC provides a programing example for the Q series programmable controller.
In the programming example for the FR-E500, the A series programmable controller is used.
The Instruction Manual of the FR-A7NC provides a programing example for the Q series programmable controller.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700