FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-Configurator
FAQ
FR-Configurator
1. Can I set the station number with the USB connection?
2. Is the COM setting given by the FR Configurator necessary?
2. Is the COM setting given by the FR Configurator necessary?
- Category :
Answer
1. You can set the station number.
However, you can only connect a single personal computer to a single inverter.
2. You can set communication by choosing Tool -> Option in the software.
The COM port setting is not necessary for USB connection.
You must specify a number for RS-232C connection.
Set the output COM port number.
(Check the port number in Device Manager on the personal computer.)
However, you can only connect a single personal computer to a single inverter.
2. You can set communication by choosing Tool -> Option in the software.
The COM port setting is not necessary for USB connection.
You must specify a number for RS-232C connection.
Set the output COM port number.
(Check the port number in Device Manager on the personal computer.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700