FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > CC-Link
FAQ
CC-Link
I am using CC-Link for the first time. Let me know which parameters need to be set on the inverter.
- Category :
Answer
Set Pr.79 (Operation mode) setting value to "0", "2", or "6", Pr.340 (Communication startup mode selection) other than the setting value, Pr.542 (Station number), Pr.543 (Baud rate selection), and Pr.544 (CC-Link extended setting).
Perform the power reset after setting the parameters.
Ensure that the "NET" LED on the inverter's operation panel turns on.
Perform the power reset after setting the parameters.
Ensure that the "NET" LED on the inverter's operation panel turns on.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700