FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > CC-Link
FAQ
CC-Link
Can I send operation commands (forward/reverse) and set parameters via CC-Link?
- Category :
Answer
Yes.
You can issue operation (forward/reverse), frequency setting, parameter read/write, and operation monitor commands.
You can issue operation (forward/reverse), frequency setting, parameter read/write, and operation monitor commands.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700