FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > Setting of "Master / slave setting switch" (Model: EMU4-D65).
FAQ
Setting of "Master / slave setting switch" (Model: EMU4-D65).
An error is indicated immediately after starting the Display Unit (Model: EMU4-D65) for the Energy Measuring Unit.
What kind of causes assumed?
What kind of causes assumed?
Answer
It is assumed that setting of "Master/Slave setting switch" at the bottom of the Display Unit (Model: EMU4-D65) for the Energy Measuring Unit is wrong. Perform settings as below depending on usages.
1. Set "Master (switch 1: OFF, switch 2: OFF)" where one Display Unit is connected to one Energy Measuring Unit.
2. Set one of Display Units as "Master (switch 1: OFF, switch 2: OFF)", other Display Units as "Slave (switch 1: ON, switch 2: OFF)" where plural (Maximum 7 units) Display Units are connected to one Energy Measuring Unit.
1. Set "Master (switch 1: OFF, switch 2: OFF)" where one Display Unit is connected to one Energy Measuring Unit.
2. Set one of Display Units as "Master (switch 1: OFF, switch 2: OFF)", other Display Units as "Slave (switch 1: ON, switch 2: OFF)" where plural (Maximum 7 units) Display Units are connected to one Energy Measuring Unit.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus
May I have your opinion?
Related FAQ
- As to the current sensor usable for the EcoMonitorPlus (Model: EMU4-BM1-MB, EMU4-HM1-MB, EMU4-A2, EMU4-VA2).
- Simultaneous data acquisition of MODBUS RTU communication and Optional Unit.
- Cause of "minus" indication for electric power value (EcoMonitorPlus/Light).
- As to simple measuring function of the EcoMonitorPlus (Model: EMU4-BM1-MB、EMU4-HM1-MB、EMU4-A2、EMU4-VA2).
- As to timing for outputting data file into the SD memory card.