FAQ


FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > As to timing for outputting data file into the SD memory card.
FAQ
As to timing for outputting data file into the SD memory card.
When is the time to output data file from EMU4-LM into the SD memory card?
Answer
EMU4-LM outputs data file at following timing.
1. When inserting the SD memory card while operating.
2. When power is ON in a state of the SD memory card inserted.
3. At every hour on the hour while operating in a state of the SD memory card inserted.
1. When inserting the SD memory card while operating.
2. When power is ON in a state of the SD memory card inserted.
3. At every hour on the hour while operating in a state of the SD memory card inserted.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus, EcoMonitorLight