FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > How to set battery-less operation(FX3U/FX3UC)
FAQ
How to set battery-less operation(FX3U/FX3UC)
Are there any settings for battery-less operation in the FX3U/FX3UC series?
- Category :
-
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Accessories
Answer
To perform battery-less operation in the FX3U/FX3UC series, set parameters using GX Works2(or GX Developer).
Please refer to the following manual for further details;
FX3U SERIES PROGRAMMABLE CONTROLLERS USER'S MANUAL(Hardware Edition)
9.3.2 Setting the battery mode
If you wish to set this operation by using a sequence program, please refer to the following manual for further details;
FX3S/FX3G/FX3GC/FX3U/FX3UC SERIES PROGRAMMING MANUAL - Basic & Applied Instructions Edition
37.2.10 Battery [BATT (BAT)] LED and [ALM] LED OFF command [M8030]
Please refer to the following manual for further details;
FX3U SERIES PROGRAMMABLE CONTROLLERS USER'S MANUAL(Hardware Edition)
9.3.2 Setting the battery mode
If you wish to set this operation by using a sequence program, please refer to the following manual for further details;
FX3S/FX3G/FX3GC/FX3U/FX3UC SERIES PROGRAMMING MANUAL - Basic & Applied Instructions Edition
37.2.10 Battery [BATT (BAT)] LED and [ALM] LED OFF command [M8030]
- Product Name
- FX3U, FX3UC
- Product Category
- Main unit, Accessories, Options, Engineering Software, GX Developper, GX Works2
- Series
- FX3U, FX3UC