Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23558
  • Release Date : 2018/09/14 15:09
  • Print

Battery error

Answer

The following shows the devices for the battery errors.
• [SM51] Battery low latch
  Turn ON when the voltage of battery reduces to less than 2.5[V].
  Remains ON even if the condition is restored to normal thereafter.
• [SM52] Battery low
  Turn ON when the voltage of battery reduces to less than 2.5[V].
  Turn OFF when the voltage of external battery returns to normal.
• [SM58] Battery low warning latch
  Turn ON when the voltage of battery reduces to less than 2.7[V].
  Remains ON even if the condition is restored to normal thereafter.
• [SM59] Battery low warning
  Turn ON when the voltage of battery reduces to less than 2.7[V].
  Turn OFF when the voltage of external battery returns to normal.
Product Name
Motion controller
Series
MELSEC-Q

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries