FAQ


FAQAbout Products

- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDCPU > Error 2035
FAQ
Error 2035
What is error 2035?
What should I do when it occurs?
What should I do when it occurs?
- Category :
-
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDSCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MSCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nHCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nCPUN
Answer
Error 2035 (Command frequency error) occurs when the servo amplifier detects a command frequency error.
(1) When the command is the permissible speed or higher. Check operation pattern.
(2) When the command is lower than the permissible speed.
• Take countermeasure against I/O signal noise
• Take countermeasure against servo system controller noise
Refer to relevant servo amplifier manuals for details.
(1) When the command is the permissible speed or higher. Check operation pattern.
(2) When the command is lower than the permissible speed.
• Take countermeasure against I/O signal noise
• Take countermeasure against servo system controller noise
Refer to relevant servo amplifier manuals for details.
- Product Name
- Motion controller
- Series
- MELSEC-Q