FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Controllers > Motion Controllers > MELSEC iQ-F Series > Simple Motion Modules > FX5SSC > Servo status
FAQ
Servo status
Can I check the servo status with the Simple Motion module?
- Category :
Answer
Yes. You can check the servo status through the following monitor data.
• "[Md.108] Servo status 1"
• "[Md.119] Servo status 2"
• "[Md.125] Servo status 3" (RD77MS, FX5_SSC-S)
• "[Md.108] Servo status 1"
• "[Md.119] Servo status 2"
• "[Md.125] Servo status 3" (RD77MS, FX5_SSC-S)
• "[Md.126] Servo status 4" (RD77MS)
• "[Md.127] Servo status 5" (RD77MS)
• "[Md.500] Servo status 7" (RD77MS, FX5_SSC-S)
• "[Md.500] Servo status 7" (RD77MS, FX5_SSC-S)
- Product Name
- Simple Motion module
- Series
- MELSEC iQ-R, MELSEC iQ-F