FAQ


FAQAbout Products
- FAQ > Controllers > Motion Controllers > MELSEC iQ-F Series > Simple Motion Modules > FX5SSC > Warning 093EH
FAQ
Warning 093EH
What is warning 093EH?
What should I do when it occurs?
What should I do when it occurs?
- Category :
Answer
Error 093EH (SSCNET communication error) occurs when erroneous data is received from servo amplifier.
[When the servo parameter "[PA14] Rotation direction selection/travel direction selection" is changed]
Execute the home position return again.
[When the servo parameter "[PA14] Rotation direction selection/travel direction selection" is not changed]
• Check if the SSCNETIII cable and the encoder cable are connected correctly.
• Take measures against noise.
[When the servo parameter "[PA14] Rotation direction selection/travel direction selection" is changed]
Execute the home position return again.
[When the servo parameter "[PA14] Rotation direction selection/travel direction selection" is not changed]
• Check if the SSCNETIII cable and the encoder cable are connected correctly.
• Take measures against noise.
- Product Name
- Simple Motion module/
Positioning module
- Series
- MELSEC iQ-R
MELSEC iQ-F