Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23630
  • Release Date : 2018/09/14 15:10
  • Print

Encoder resolution during J3 compatibility mode

I use the MR-J4-B servo amplifier in J3 compatibility mode.
I use it in combination with the HG series servo motor and what is the encoder resolution?
Category : 

Answer

18 bits (262,144 pulses/rev.)
The encoder resolution of HG series servo motor in J4 mode is 22 bits (4,194,304 pulses/rev).
For details of J3 compatibility mode, refer to each servo amplifier instruction manual.
Product Name
AC Servos-MELSERVO
Series
MELSERVO-J4, MELSERVO-JE
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?