FAQ


FAQAbout Products

- FAQ > Drive Products > AC Servos-MELSERVO > MELSERVO-J4 > Encoder resolution during J3 compatibility mode
FAQ
Encoder resolution during J3 compatibility mode
I use the MR-J4-B servo amplifier in J3 compatibility mode.
I use it in combination with the HG series servo motor and what is the encoder resolution?
I use it in combination with the HG series servo motor and what is the encoder resolution?
- Category :
Answer
18 bits (262,144 pulses/rev.)
The encoder resolution of HG series servo motor in J4 mode is 22 bits (4,194,304 pulses/rev).
For details of J3 compatibility mode, refer to each servo amplifier instruction manual.
The encoder resolution of HG series servo motor in J4 mode is 22 bits (4,194,304 pulses/rev).
For details of J3 compatibility mode, refer to each servo amplifier instruction manual.
- Product Name
- AC Servos-MELSERVO
- Series
- MELSERVO-J4, MELSERVO-JE