FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > AC Servos-MELSERVO > MELSERVO-J3 > Parameter group is not displayed.
FAQ
Parameter group is not displayed.
I want to use HG-AK motor with MR-J3W-0303BN6. However, the parameter PO group is not displayed. How can I see the PO group?
- Category :
Answer
Some parameters are write-protected. (MR-J4/MR-J3: PA19)
The parameter to be displayed is determined by the setting value of this parameter.
Do as follows for MR Configurator2.
Method 1:
Set PA19 to “000E” in the list display and perform the parameter reading after writing PA19 to the servo amplifier (servo amplifier power supply OFF/ON).
Method 2:
Set PA19 to “000E” in the parameter block and click “initial setting” button.
The parameters other than PA19 are initialized.
The setting value “000E” differs depending on the parameter reference/writing range.
- Product Name
- MR Configurator2
- Series
- MELSERVO-J4, MELSERVO-J3