FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > How to measure circuits over 600A (EcoMonitorPlus / Light)
FAQ
How to measure circuits over 600A (EcoMonitorPlus / Light)
How to measure circuits over 600A with an Energy Measuring Unit (EcoMonitorPlus / Light)?
Answer
As shown in the figure below, a current transformer (CT) with a secondary current of 5A is attached to the measurement location, and a split-type current sensor for the Energy Measuring Unit (model name: EMU-CT5-A, EMU2-CT5, EMU2-CT5-4W) is installed on the secondary side of the CT.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitorPlus, EcoMonitorLight
May I have your opinion?
Related FAQ
- Pulse magnification setting of EMU4-PX4(Pulse Input Unit)
- Branch connection for MODBUS RTU communication
- Setting of "Master / slave setting switch" (Model: EMU4-D65).
- EcoWebServerIII's rated voltage value setting with VT connections
- Checking the disconnection or communications error status of the Energy measuring Unit