FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Automation Controllers MELSEC > MELSEC MX Controller MX-F Model > Regarding connectable I/O Modules
FAQ
Regarding connectable I/O Modules
Which I/O Modules can be connected to the MX-F Model?
Answer
It is possible to connect the I/O Module of the MX-F Model to the extension cable type I/O Module of the iQ-F series.
To connect an extension cable type I/O Module of the iQ-F series, you need a connector conversion Module: FX5-CNV-IFC or an Extension power supply module: FX5-C1PS-5V.
MX-F Model I/O Module List

iQ-F Series I/O Module List

- Product Name
- MX-F Model
- Series
- MELSEC MX Controller