FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Automation Controllers MELSEC > MELSEC MX Controller MX-F Model > Regarding number of expansion adapter connections
FAQ
Regarding number of expansion adapter connections
How many expansion adapters can be connected to an MX-F Model?
Answer
The number of expansion adapters varies depending on the type of adapter, and up to six can be connected.
・Analog adapter: Up to 4
・Communication adapter: Up to 2

- Product Name
- MX-F Model
- Series
- MELSEC MX Controller