FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Automation Controllers MELSEC > MELSEC MX Controller MX-F Model > Regarding maximum number of connected stations for built-in CC-Link IE TSN
FAQ
Regarding maximum number of connected stations for built-in CC-Link IE TSN
What is the maximum number of connected stations for the built-in CC-Link IE TSN of MX-F Model?
Answer
The maximum number of stations that can be connected in the network depends on the model name of the MX-F model.
・MXF100-16 N32/P32: Up to 46 stations
・MXF100-8 N32/P32: Up to 38 stations
- Product Name
- MX-F Model
- Series
- MELSEC MX Controller